REGEN.POWER

General Information

Type

R/O parameter

Description

Reads regen resistor's calculated power.

Units

Watt

Range

N/A

Default Value

N/A

Data Type

Integer

See Also

N/A

Start Version

M_01-00-00-000

Description

This parameter reads regen resistor's calculated power, which is determined as follows:

(V2 / R) * DutyCycle

Related Topics

Regeneration

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™